Part Number: LM25143-Q1 Other Parts Discussed in Thread: LM5143
Hello team,
we operate the LM5143 in single output(3.3V) 6-phase mode. How to the wire of the slave controllers?
This is the information provided in datasheet. How to provide 0, 60, 120 degree…
Part Number: LM25143-Q1 Hello Texas Instruments,
Good Day!!!!!!!!!
In the datasheet we can't able to find the maximum channel current of LM25143-Q1. Just wanted to know what can be the maximum current of both channels(VOUT1 & VOUT2)
Thanks for…
Part Number: LM25143-Q1 Hi Team,
May I know the VFB-REG voltage variation under -40oC to 85oC TJ & TA?
The data listed in the datasheet is based on 25oC TJ.
Or the VFB-REG range works for -40oC~150oC TJ?
Thank you.
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM25143-Q1 , LM5143 , LM25143 Hello,TI experts
For LM5143-Q1 AND LM25143-Q1 ,could you help to ask to me different points.
I only find input range is different,they are whether is pin to pin?
Part Number: LM25143-Q1 Other Parts Discussed in Thread: LM5143 Hi TI team,
Good evening.
Kindly review the schematic of Buck converter using two LM5143 ICs.
Input:36V
Output:2V to 24V variable voltage with 30A single output.
We can obtain the variable…
Part Number: LM25143-Q1 Other Parts Discussed in Thread: PMP31202 , LM5143DESIGN-CALC , LM5143 PMP31202-Schmatic.pdf
Hi TI team,
Good evening.
We have designed the buck converter using LM5143QRWGRQ1 IC with below specification
Input Voltage: 36V
Output Voltage…
Part Number: LM25143-Q1 Hello,
my question is on the max rating of SW1/2 of LM25143-Q1. Currently they are specified with -0.3V.
Wouldn't this be an issue, in case LOL1/2 gets open?
Thanks and best regards,
Michael
Part Number: LM25143-Q1 Other Parts Discussed in Thread: LM5143-Q1 , LM5143 , LM25143 , LM5143-Q1EVM-2100 Hi team,
I have some questions here.
1. LM25143-Q1 can be designed as spec LM25143-Q1?
2. Since this part number is discrete solution and no EVM. if…
Part Number: LM25143-Q1 Other Parts Discussed in Thread: LM25143 We want to make to 20v and 20a Single-Output Interleaved Operation by using LM25143.
But we tried to use Webench design tool and it showing error like,
Your preferred device does not work…