Part Number: TIDA-010006 Other Parts Discussed in Thread: LM5180 Hi,
We have a customer whose requirements are similar to TIDA-010006, below are their requirements.
Input: DC20V +/-10%
Output 1: DC20V/120mA.
Output 2/3/:DC15V/50mA each of them.
…
Part Number: LM25180 greetings, When the LM25180 chip is used, the output is unstable at 12v input, and the target output voltage (5v) cannot be reached when the load is more than 100mA. The output is basically stable when the input voltage is increased…
Part Number: LM25180-Q1 Hi,
The customer will review the LM25180-Q1 for the inverter project.
Please share your email for a private Schematic review.
Operation : 9-16V / Vo = 18V
DCLINK : 800V Spec 1 : U/V/W typ : 0.2A
UVWL typ : 0.6A Spec 2 :
U/V/W typ…
Hi Brian,
The reason we recommend a lower inductance value is that besides having a high leakage inductance, the part rating you select for the RC snubber or flyback diode will also have to be higher, which would increase cost. Another thing to watch out…
Part Number: LM25180-Q1 Other Parts Discussed in Thread: LM25180 , Hello,
We are using an LM25180-Q1 to to generate +/- 15 output supplies. While using the LM25180 PSR flyback quickstart design tool, the Minimum Magnetizing Inductance is given as 23.0 uH…
Part Number: LM25180-Q1 Other Parts Discussed in Thread: LM25180 , LM25184 , LM25183 Hello experts,
I want to use LM25180-Q1 in my new project. My input is 8-15V, output is 12.5V 1.5A >15W isolated output. but When I tried on WEBENCH, it showed…