Part Number: LM25183 Other Parts Discussed in Thread: UCC14241-Q1 , UCC15241-Q1 Tool/software: HI team,
Could you help check if we have alternative of MID1W2424A?
24-24V, 1.5W, Isolated DC/DC Converter With 5kV RMS Reinforced Isolation, with an integrated…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM25183-Q1 , , LM25183 Hi Sir,
My customer is looking for a isolation power devices to meet the ISO 7637 standards, and the power spec V-in is 9~36V, V-out is 12V, I-out is 2A. They found these devices…
Hello Shritesh,
We have a high-accuracy, soft-start timer in the IC.
6ms (internally fixed). It can also be programmed externally with a soft-start cap.
There are also a couple startup waveforms if you want to see what the device signature looks like …
Part Number: UCC28C50-Q1 Other Parts Discussed in Thread: LM5180 , LM25183 Hi Team,
I'm looking for designing an isolated bi-polar power supply with fly-back topology for my Mosfet Gate driver circuit. I'm little confused on selecting right controller…
Hi John,
Your issue with the load is mostly related to running into the 420ns. The 20% is in the datasheet, at the end of section 7.3.2. Here I copied and paste below from the LM25184-Q1 datasheet, because the LM25184 industrial version datasheet has…
Part Number: LM25180-Q1 Other Parts Discussed in Thread: LM25180 , LM25184 , LM25183 Hello experts,
I want to use LM25180-Q1 in my new project. My input is 8-15V, output is 12.5V 1.5A >15W isolated output. but When I tried on WEBENCH, it showed…
Other Parts Discussed in Thread: UCC28C43-Q1 , LM25183-Q1 , LM25183 , UCC28C43 I want to design 24 volt to 5v/3a and 3.3v/3a isolated power supply for rhe automative applicatiobn. which IC should be preferred.
Hi Nihan,
I have looked at our portfolio and i did not see a ready to use module with isolation and the desired specifications.
One product that may work is LM25184 or LM25183 which is a PSR Flyback design but they are also not in stock unfortunately…
Part Number: LM25184-Q1 Other Parts Discussed in Thread: LM25184 , LM5155 , LM5156 Hello,
We would like to use LM25184-Q1 in our fly back design.
specification :
Input voltage : Min :12V , Normal :15v ,max :17V
Output voltage :15V 1A and 7V .25A
Inductance…
Part Number: LM25184-Q1 Tool/software: Hi team,
Could you please help review below schematic and give some suggestions? Thanks!
7115.LM(2)518x PSR flyback converter quickstart tool revB.xlsx
Regards,
Ivy