Part Number: LM25190 Other Parts Discussed in Thread: LM654B0-Q1 Hello,
I am searching for a CC-CV part that can deliver high power (50W to 100W). I have used the LM25190 to deliver ~10W but have not tried pushing it past this point.
Operating CV…
Part Number: LM5190QEVM-400 Other Parts Discussed in Thread: LM25190 Good morning,
I would like to ask whether it is possible to obtain the design files (schematic and PCB layout) of the evaluation board in Altium Designer format. I would need them…
Hi Piet,
The LM25190 42V-rated version is the way to go here, as it has the integrated CC loop and is not that complex. However, if you need a converter (with integrated FETs) and can add an external CC loop, then take a look at the LMR60440, LMR51440…
Hi Nicole,
Yes that datasheet looks incomplete. For I would encourage you to used the user guide and the QuickStart calc until this issue is being resolved. 5428.LM5137-Q1_quickstart_calculator_revB6.xlsm and 7266.snvu891.pdf
Hi NATH
The LM25190 has an input voltage of approximately 15.3 Vdc. The circuit diagram and the Excel tool are attached for reference.
3157.SCH.pdf
LM5190.xlsx