Part Number: LM25576-Q1 Hi,
the maximum value is mentioned as -1.5V For creating a 5V, SW to GND value will definitely be higher than 0V.
Could you please confirm this value?
Part Number: LM25576 Hello,
I am using LM25576 in inverting Buck-Boost configuration to generate -12.5V from 12V. I wanted to know if this device will be capable of sourcing any current in this configuration?
Thanks
Part Number: LM25576 Hi Team,
While I was watching TI training video , I found the sch below. Could you please explain why there's a diode (D2) from OUT to VCC? I wasn't able to find any information from DS and EVM guide.
Thank you.
Part Number: LM25576 Hello,
I am trying to adjust the output voltage of the LM25576, circuit attached. It runs off +/-16V, and boosts up to a high voltage, however the regulator main output needs to be 12V
Unfortunately the output is fixed to around…
Part Number: LM25576 Hi, team.
The overcurrent protection value of the LM25576 data sheet (SNVS470H) is too small.
Typ 2.1A, Min 1.8A, Max 2.5A
Is it a typo?
Part Number: LM25576 Posting this on customer behalf:
Currently using the LM25576 in an inverting configuration (6V25 to -15V @ 400mA)
We’re using comparable ceramic caps (45uF, and similar ESR) to the Tantalums, but there are stability concerns if…
Other Parts Discussed in Thread: LM25576 Hello,
I need to add a 10F Supercap on 5V output of the LM25576 of an existing design. The LM25576 is fed by 12V.
I read some posts for other devices:
http://e2e.ti.com/support/power_management/non-isolated_dcdc…
Other Parts Discussed in Thread: LM25576 Our production device is powered by an LM25576 circuit virtually identical to the reference design. We expect 12v in with wide allowance, and produce 5v out. Our device has a USB port but we have not used the available…