Part Number: LM2574 On the LM2574 datasheet (page 4) in the absolute maximum specification it has the output voltage to ground steady state voltage rating.
I'm wondering if there is a transient output voltage pin undershoot maximum? For most switching…
Part Number: LM2574HV Other Parts Discussed in Thread: LM2574 Hello,
I am currently planning on using the LM2574HV adjustable switching regulator to regulate 24V input down to 5V, no more than 0.1A needed on output. However, we also need the ability to…
Hello
The LM2597 can be used, however the DELAY pin must be left floating.
Another option is the LM2674; you need one extra capacitor for that device.
The LM2574 is another option but it is not P-to-P.
The TPS54321 seems to be in stock; but again is not…
Part Number: LMZ34002 Other Parts Discussed in Thread: LM2574 , Hello,
I have LMZ34002RKGT DC-DC converter and TPS7A3001MDGNTEP LDO. Should I use heatsink with this parts?
Thank you in advance.
Sincerely,
Behtan Umut Mercan
Part Number: TL2575-05 Other Parts Discussed in Thread: LM2574 , LM2674 , LM2675 , LM22675
Hello,
I'm considering to use a TL2575 for a application with the following values:
Vin = 24V
Vout = 5V
Iout = 375mA
From the Graph on the datasheet (Figure 14…
Hi Josiah,
the LM2674 is directly driving the fan. Not as a pre-regulator. We had to add the fan afterwards, after the project was already finished. We had a 18V supply and decided to add a 5V Fan to it, powered by a LM2674 switcher. The LM2674 has a…
Other Parts Discussed in Thread: LM2574 , TPS62125 Dear Sir
i have search LM2574, this part is similar, but seems can't be Vin5V to Vout-5V.
May you have suggest DC2DC part that suit use in audio 5Vin -5Vout/100mA application?
…
Benjamin,
The LM385BLPR-1-2 should drop in for the LT1004CLP-1-2. You may want to start a new thread for the LM2574 with the part number in the subject line.