Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LM2576HV Issue: Customer use LM2576HVS-5.0 as the adjustable version to output adjustable voltage.
When the input voltage is 48Vand the setting output voltage exceed 40V, the power dissipation of this IC is unexpectedly high, in some…
Part Number: LM2576HV I would like technical support to understand the damage of the diode in the buck regulator circuit. The circuit is converting VIN: 50V to VOUT: 5V with a current of 100mA.
The diode used is PN: SB5100 of 100V / 5A. I am using this…
Part Number: LM2576HV Hi there, a customer highlighted this, can you please tell me what is the actual number for Vout....MAX at 25C? The Red circle below. Max is lower than nominal (4.75V).
Device: LM2576HVT-5.0/NOPB
Part Number: LM2576HV Tool/software: WEBENCH® Design Tools I used Webench to design a regulator from 30-60V to 12V, 2.1A.
The recommended inductor is Wurth 74437529203331.
This item is usually not stocked, and with long lead time.
But the Webench didn…
Part Number: LM2576HV hello, We use a LM2576HV-Adj IC for power supply. Cin 100uf/ Cout 330uf/ L 330uH/ Diode SK39A/ Vin 60V/ Vout 12V. we used one switch for on/off the output voltage. we connect pin5 of LM (ON/OFF pin) with R 4.7K to Vin and with Switch…
Part Number: High spark with high voltage IC-LM2576HV Hi I use a LM2576HV IC at an input voltage of up to 60 volts, a output of 5 volts and 1 amp. Output capacitor 470uf, input capacitors 100uf, inductor 100uh and 3amp schattky diode. When I connect voltages…
Part Number: LM2576HV Hello I have an idea about the input protection circuit. You used a protective circuit like a diode TVS! But you can be sure that it will work! Does it really protect against voltages above 60 volts? It is best to disassemble the IC…
Dear Sir,
I am using LM2576HVS-ADJ/NOPB to power the IC UC3526DW. Input Voltage: 24V DC LM2576HVSADJ.pdf Output Voltage: 12 V DC Current Max: 1A
My voltage output waveform is not clean having some switching noise observed on DSO. Please verify my schematic…
Part Number: LM2592HV Other Parts Discussed in Thread: LM2576HV , Tool/software: Hi,
I need to replace the components of a LM2576HV TO220 based buck power supply with these specs Vin: 48V, Vout:45V, Iout:1.5A I would like to use an LM2592HV which would…
Part Number: LM2576HV Tool/software: WEBENCH® Design Tools I would like to know if the problem has been resolved I am having the same case and would like help