Part Number: LM2585 Hi,
I plan to use LM2585 to convert input 24V to 300V. In WE bench I have got the simulation results which is shown below. I have a query regarding transformer ratio.
In the BOM the transformer specification is mentioned as below: …
Part Number: LM2585 Hello,
I am struggling to find a suitable transformer for the LM2585. My needs are as follows:
1- input voltage 24V;
2 -output voltage 60V;
3- configuration: flyback;
4- power: 20W output
Currently I am using the WE 750313976, which…
Part Number: LM2585 Hi,
I am using the LM2585-ADJ to generate a 49V Phantom voltage from a 18V input voltage.
The current drawn is only 10mA max so power dissipation will not be significant.
Still, to keep the design as cool as possible I want to add…
Part Number: LM2585 Hi Team,
One of my customer is facing issues with device during output short circuit test. The flyback output is designed for 15V/1.2A from 24V input. For UL safety tests the output is shorted and observed that the device current is…
Part Number: LM2585 Other Parts Discussed in Thread: TPS55340 Hi team.
My customer needs the Pspice model for LM2585.
If you have it, could you share it to me?
I can not found in your site( http://www.tij.co.jp/ja-jp/design-resources/design-tools-simulation…
Part Number: LM2585 Hi team,
Good day.
How to calculate for the compensation network of the LM2585? I have seen below application report, is it also applicable for LM2585? www.ti.com/.../slva452.pdf
Thank you in advance for the help. Regards, Carlo
Part Number: LM2585 Hello,
I search a spice model for LM2585 to simulate it with a software for a project.
Thank you by advance for your help,
Have a good day,
Part Number: LM2585 Hi team.
I have some questions about the internal logic for LM2585.
My customer refer to snva005b(p.7) and configure the flyback.
1. About the soft start.
If a momentary power failure occurs and the input voltage has a residual voltage…
Part Number: LM2585 Tool/software: WEBENCH® Design Tools
Hey,
We would like to know the possibility of the availability of the above design in Webench since we found the above same design in one of the documents related to LM2585 which was provided by…