Part Number: LM2598 Is it possible to use the LM2598 in an application with 5-36V in, 5V out?
It mentions a max duty cycle of 100%, does that mean this mode of operation is supported?
Hi Ales,
Instead of using LM2595, you might be able to use the LM2598 which has a soft-start pin.
http://www.ti.com/product/lm2598/description
In this case you can adjust the value of the capacitor in order to set the output voltage rate that…
The soft-start for the LM2596 is fixed and not specified. We can not guarantee that it is longer than 200us
However, the LM2597 or LM2598 both have adjustable soft-start; one of these may be a better choice.