Part Number: LM2611
Tool/software:
Dear Expert I need various output voltages from a single input supply in my ADC-DAC design. This can be done with different products and designs. I kindly ask you to help me which products and designs to use in terms…
Part Number: LM2611 Tool/software: I tried to generate -20V DC output voltage with +5V input with LM2611 EVM and LM 2611 with similar circuit design.
When i use a power supply with current limit setting more than 1.5A. It can generate -20V well with…
Part Number: LM2611 Hi Experts,
LM2611 is mass production on customer side. There is a issue when they testing it:
1. When the supply voltage under 2.5V(less than the minimum working voltage), the the SW is short to ground, is it the normal status…
Hi Niklas,
While debugging, I have found the below observation:
Case 1: With the SHDN pin connected to the VCC directly, If I supply 12V at the input to the regulator, the output voltage of the regulator is -4.88V. When I connect a load at the -5V…
Part Number: LM2611 Hello Team,
I can see the Grade A and B have difference in Current limit value.
Is there any reason LM2611 has 2 kinds of current limit? Thank you!
Part Number: LM2611
Hi team, Kindly review the schematic above motioned , I have used the inductor part CR32NP-150KC Kindly share your feedback..
Thanks Arun
Part Number: LM2611 Hello,
despite searching effort I have not found any clear answer, what this parameter on the p. 10 of the LM2611 datasheet stands for.
Could you please help me with this one? According to general convention, it shall be some kind…