Part Number: LM2611 Tool/software: WEBENCH® Design Tools It is the device I want to simulate, but no matter what I/Os I enter, it is never an option.
It would be nice if one of the options when setting things up is the ability to select the device we…
Part Number: LM2611 I'm implementing a +5V to -20V regulator with an output current requirement around 10-20 mA. Because of the low current, I'm anticipating that pulse-skipping mode may kick in, which I want to avoid to decrease ripple. I've currently…
Part Number: LM2611 Please let me know about two points below for Hysteretic mode function;
①Condition of enter Hysteretic mode
For example, inductor ripple current reached 0A, or reached minimum on time, etc.
②Spec for minimum on-time
Best regards…
Part Number: LM2611 I have a question about LM2611 datasheet page 8, figure 13.
About output side of figure 13, I think that polarity of Vout side are upper side (between L2 and Vout):plus and lower side (between Vout and GND):minus.
But datasheet is…
Part Number: TPS552892-Q1 Other Parts Discussed in Thread: TPS552892 , LM2611 , LM5157 , , LM63635-Q1 Hello,
I am looking for a schematic - using the TPS552892- converting positive voltage (12V) to a Negative Voltage (-15V) .
Regards,
Giora
.
Part Number: TPS6735 Other Parts Discussed in Thread: TPS61085 , LM2611 Can I use TPS6735 to design -30VDC output for <50mA power supply? Does TI have a design example to use?
Other Parts Discussed in Thread: TINA-TI , MC34063A , LMR51420 , LM5146 , LM2611 , TPS54561 Good day team,
I need to simulate a negative 30VDC output from a 12V battery input using TINA-TI. I have been looking for TINA-TI simulation files of various Buck/I…
Part Number: LM2611 Hi
My customer evaluate LM2611.
But this device broke when they used this device slowly started up(a few seconds to a few tens of second).
They used this device under Vin=5V and Vout=-5V.
If this device is used the low Vin, is there…