Part Number: LM2623 Other Parts Discussed in Thread: TPS61376 Does TI have a boost chip similar to the LM2623?
Input voltage 0.9-16V, but But it's cheaper than the LM2623.
Part Number: LM2623 I am finding a replacement material for AP3015KTR-G1(Diodes), witch price is 1.9USD, so aggresive.
Cusotmer need input voltage is less than 1.5V and the output voltage is greater than 12V.
Do we have any recommendations?
thanks…
Part Number: LM2623 To whom it may concern,
I am working with the LM2623 for my current design. I am wondering what parameters for capacitor C1 and C2 are suggested for operation? Also, is it recommended that a tantalum capacitor be used or a ceramic…
Part Number: LM2623 Other Parts Discussed in Thread: TPS61022 Hi,
In the datasheet mentioned that the maximum voltage for VDD is 5V and the absolute maximum rating is 10V.
i would like to ask how much is it problematic to push the VDD voltage of 5…
Part Number: LM2623 Other Parts Discussed in Thread: LM2735 Hi TI
I am having trouble using the LM2623A to step up from 5V (USB) to 12V with output current up to 500mA.
The issues I am having are:
1) Large input current ripple causing big…
Part Number: LM2623 Other Parts Discussed in Thread: LM2621 , LMR61428 Hello,
I was hoping I could get some help choosing the right TI part. I need a boost converter for a 2cell AA battery application.
Vin min = 1.8
Vin max = 3.1
Vout = 8V…
Part Number: LM2623 To whom it may concern. I have a few questions regarding the LM2623. First, I am wondering what the difference between LM2623MM/NOPB and a regular LM2623. What is the difference. Also, I have routed my PCB with a clearance of 10mil…
Part Number: LM2623
I am designing with the LM2623A controller.
Vin min = 1.8V
Vin max = 4.5V
Vout = 9.5V
Iout = 0.2 A
In the datasheet, it says selecting C3 is a "trial and error" process. But I was hoping to get some guidance as to what…