Part Number: LM26420 https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1170998/lm26420-q1-short-circuit-to-ground
I'm having the same problem. Could you share your conclusions?
Part Number: LM26420-Q1 Other Parts Discussed in Thread: LMR43620 Hello team,
Can you teach me for SN29500 component type of this device?
For example LMR43620 datasheet, there is mentioned in Pin FMEA document.
Regards,
Youhei MIYAOKA
Part Number: LM26420-Q1 Tool/software: Hello Expert,
Could you please tell me Absmax rating and recommended operating range of PG pin? As far as I confirmed, There isn't this rating.
Best regards, Kazuki Kuramochi
Part Number: LM26420-Q1 Tool/software: Hello Expert,
Could you please tell me Absmax rating and recommended operating range of PG pin? As far as I confirmed, There isn't this rating.
Best regards, Kazuki Kuramochi
Part Number: LM26420-Q1 Tool/software: Hello Expert,
Could you please tell me PG pin Absmax rating and recommended operating range of PG pin?
As far as I confirm datasheet, there isn't any specification.
Best regards, Kazuki Kuramochi
Part Number: LM26420-Q1 Other Parts Discussed in Thread: TPS62442-Q1 Tool/software: I am working with the DC/DC converter LM26420Q1XMHX/NOPB. I need a converter similar to this one with two inputs and the two channels are independent.
Part Number: LM26420-Q1 Other Parts Discussed in Thread: LM26420
LM26420-Q1.
Our product uses two LM26420-Q1. When we separately measure the static current of LM26420-Q1, the sum of the static current of VINC and VIND is 24mA, which is basically close…
Part Number: LM26420-Q1 Hi Team,
Could you possible hlep to share if we have dual channel device which could support 3.3V input voltage, and ≥ 2.5A for each output channel, output voltage should 1.1V and 1.8V. Thanks a lot for your support to recommend…
Part Number: LM26420-Q1 Other Parts Discussed in Thread: TPS62442-Q1 Greetings,
When I run this part through Webench , with 3.3v input, 1.0v out and 0.7amps, the phase margin drops below 35 and Webench fails with, " Design update failed. This design…
Part Number: LM26420-Q1 Thanks for your support
After the chip returned to normal temperature after a low temperature test, the chip failed.
The output voltage is less than 100mV.
The resistance between sw to GND is 5 ohm.
We guess the lower MOS…