Part Number: LM26480-Q1 Hello,
I am currently designing power circuitry using LM26480-Q1 and I have question regarding the GND separation for this chip.
As this chip has pin for core ground (GND_C) , LDO ground (GND_L) , and switching GND (GND_SW1, GND_SW2…
Part Number: LM26480-Q1 Customer's safety team came back to me with some technical questions as shown below :
- we would like to measure/verify threshold levels for UV detection at Buck1 and buck2 output. Moreover in data sheet there’re only typical…
Part Number: LM26480-Q1 Hi TI team,
I have some questions regarding the LM26480-Q1 :
- What is the maximal current that can support the open drain logic output nPOR when it is pulled to ground? it is not specified in the datasheet.
-I use this signal…
Part Number: LM26480-Q1 Other Parts Discussed in Thread: LM26480 Dear Sir,
Could you please review attached file of LM26480-Q1.
5707.power-sch.pdf
Thanks.
Part Number: LM26480-Q1 Other Parts Discussed in Thread: LM26480 , TINA-TI I downloaded the TINA-TI Spice model of LM26480. However, couldn't get the AC Analysis working using LM26480_BUCK1 TRANSIENT MODEL. Any help on this is highly appreciated.
Jenny…
Part Number: LM26480-Q1 Other Parts Discussed in Thread: LM26420-Q1 , Hello Team,
My customer asks me what is the absolute max for SW pins.
I found absolute voltage value at input pins.
However, I don't find the value for SW pins in the datasheet. …
Part Number: LM26480-Q1 Other Parts Discussed in Thread: LM26480SQ-AAEV , Hello,
When using the LM26480SQ-AAEV evaluation board and also in the implementation of my design, I observe the following:
Using an input voltage of 3.3V and with the ENLDOx tied…
Part Number: LM26480-Q1 Hi Team,
My customer is interested in LM26480-Q1
The required output sequence is below;
Vin 3.3V -> 1.8V (Back1)
Vin 3.3V -> 1.1 (Back2)
LDO1 3.3 -> 2.8
NPOR (1.8V)
Under the above condition, can ENSW2 be enabled by…
Part Number: LM26480-Q1 Dear support team
Could you provide thermal data of below condition?
◆LM26480-Q1 (only back1)
・Vin=3.3V Vout=1.2V Iout=1.4A @105℃
・Vin=3.3V Vout=1.2V Iout=1.4A @25℃
Regards
Tomohiro Nagasawa