Part Number: LM2651 I am facing the following problem:
We have a legacy device where an LM2651-3.3 is used to power flash memory and the I/O rings for an FPGA, ADC, and bidirectional level shifters. The continuous power consumption is approximately…
Part Number: LM2651 Hello,
We have a regulator designed with " LM2651MTC-3.3/NOPB" p art number and our characterization shows that the sleep mode current for this design is 250mA instead of 100mA.
Input:5V, output: 3.3V
Output capacitance: 150uF…
Part Number: LM2651 Tool/software:
I'm investigating an unusual number of failed boards containing LM2651MTC-3.3 but I'm having trouble decoding the date code / lot code on the top mark.
Top line: (National Semi Logo) 97AN6EU, or some end in DU…
Part Number: LM2651 Hi,
We are having an outside vendor up-screen the part at -55 degrees C. This part is not rated to our test temperature of -55C. The process is they install the IC into a board using a TSSOP socket and check the output voltage at…
Part Number: LM2651 Hello
I have a question about LM2651MTC. About the LM2651 .xlsx I found the reverse current(min=-10.37A) to SW PIN when powering off LM2651MTC(Vin<4V) (Please refer to the attached excel file)
It is over the Absolute Maximum Ratings…
Part Number: LM2651 Other Parts Discussed in Thread: LM2671 , Can the soft start input to the LM2651 be left floating as stated in the LM2671 datasheet? Couldn't find that in the LM2651 data.
Part Number: LM2651 Other Parts Discussed in Thread: LMR12010 , Hello team,
I have a question regarding the LM2651MTCX-ADJ/NOPB.
It has a hysteretic mode at light loads that could be a problem for my problem, depending on the load at which it drops…
Part Number: LM2651-3 Hi, Can I please get the Altium Project files for LM2651-3.3EVAL. I'm building a system with it, MSP432E401 and TSP23730.
Thanks,
Mike Timko
Part Number: LM2651
Team,
can you help to verify below schematic? We are not satisfied with the sensitivity to input voltage changes (1-2 pcs out of 10000pcs in the field are getting damaged).
input voltage: nominal 12VDC, max.: 13VDC…