Part Number: LM2660 Hi TI expert
Generating a -2Vin voltage using two LM2660, TI has a chip that can convert 3.3V to -5.2V, and chip size, peripheral circuits similar to LM2660?
Thank you!
Part Number: LM2660 Other Parts Discussed in Thread: LM2663 , Hi Team,
My customer is going to replace LM2663 with LM2660. According to the following post, if LV-pin is connected to GND LM2660 works at Fosc = 10kHz even if FC is connected to GND.…
Part Number: LM2660 The customer want to know the max output current of LM2660. (Output power capability)
In the datasheet, the output current Min is 100mA.
The Maximum V+ and out continuous output current is 120mA.
How can we understand the above…
Part Number: LM2660 Other Parts Discussed in Thread: LM2662 , , LM2776 , LM2775
Per our understanding, the LM2662 is going EOL and we think we have a drop in replacement with the LM2660, but the output current is very close to the limit of 100mA whereas…
Part Number: LM2660 Other Parts Discussed in Thread: LM2662 Hello,
Since the LM2662M is in LTB, can the LM2660 be used as a drop in replacement? It looks like the only functional difference is the lower output current rating, 100mA.
Thanks, Steph…
Part Number: LM2660 Other Parts Discussed in Thread: LM2663 , LM2662 , Hi team,
We have received the EOL notification for LM2662 and LM2663.
We are considering the LM2660 as a replacement, but will the LM2660 still be produced, 10 years or more. …
Part Number: LM2660 Other Parts Discussed in Thread: LM2662 , Hi,
My customer is evaluating the LM2660M as a replacement for the LM2660MX.
As shown in the table above, there is a difference in the output voltage. I suspect that this is due to the…
Part Number: LM2660 Other Parts Discussed in Thread: LM2904B-Q1 , , TPS709 , TPS709-Q1 , TPS7B81-Q1 , TPS7B81 Hi Team,
Could you possible help to check if we have solution which could support +12V input, and ±5V output power solution? Customer want…
Part Number: LM2660 Other Parts Discussed in Thread: LM2662 , Hi,
We are considering LM2660MX/NOPB due to the EOL of LM2662M. The main differences between LM2662 and LM2660 are the switching frequency and current rating. The conditions of use are +2…