Part Number: LM2663 Tool/software: Hi,
Please provide the junction to case and board thermal resistance for LM2663M/NOPB
Kindly do the needful
Regards,
Aboorva
Part Number: LM2663 Other Parts Discussed in Thread: LM2662 Tool/software: This part no longer appears to be EOL, or is it just this version (LM2663MX/NOPB) that is still active/available?
Part Number: LM2663 Other Parts Discussed in Thread: LM2660 , LM2775 Hi Team,
Since the LM2663 has entered EOL/last time buy, is there a direct replacement that you recommend? The LM2660 is only capable of 100mA and the design requirement is >100mA…
Part Number: LM2663 Other Parts Discussed in Thread: LM2660 , TL7660 Hi, customer uses the LM2663MX and is searching for a ptp alternative. May be the LM2660 would work but in his current design the pin 1 is connected GND. Woudl that work with the LM2660…
Part Number: LM2663 Other Parts Discussed in Thread: LM2660 Hi,
One of my cusotmer is using LM2663MX/NOPB in their production project. They have asked for the thermal data for this device. In datasheet only Theta Ja is mentioned & nothing else is…
Part Number: LM2663 Other Parts Discussed in Thread: LM2662 , LM2660 , TL7660 , MAX660 Hello,
Currently, the LM2662/3 is in LTB state.
The P2P products with the same package that I found when ignoring the usage specifications and the number 1 PIN…
Part Number: LM2663 Hello,
My customer is using the LM2663 as a voltage inverter below. They have a few questions about C1 capacitor.
1. What is expected when C1 is open ?
2. What is expected when C1 is short ?
3. What is expected when C1 Cap…
Part Number: LM2663 Hello,
My customer supplies the gate bias of the GAN TR by converting the 5V input to -5V with the LM2663.
If the customer accidentally operates the SD pin without connecting it to GND, can this cause a damage inside or outside…
Part Number: LM2663 Other Parts Discussed in Thread: LM2662 The LM2663 datasheet says the SD pin is connected to GND, but does that mean there must be an external GND connection?
The sample schematics in the datasheet do NOT show an external GND connection…