Part Number: LM2670 I am planning to use LM2670 as a basic switching controller for different loads (from 400 mA to 2.5 A) using the same PCB layout. Of course, I will choice a Catch diode and an output capacitor for the worst case (Vout = 15 V @ Iout…
Part Number: LM2670 I intend to use the LM2670 for a buck converter design Vin = 26 to 34V Vout fixed 12V I = 3A
when I vary the input voltage on a fixed load, the current rises normally, then is limited to 300mA to 500mA , the more I raised the input…
Part Number: LM2670 Hello,
I am using the LM2670X-ADJ IC in a buck boost configuration successfully. The schematic is attached below for you. I need to be able to enable and disable this IC. How can I do this?
The datasheet excerpt is also given below…
Hi Herman,
I could use your design specifications and generate & simulate the WEBENCH design without any issues from LM2670 product folder. I just used VINmin = 22V and VINmax = 26V so that actual VIN set by you comes to be 24V. I have shared link…
Part Number: LM2670 Hello guys,
One of our customers is evaluating LM2670 for DC/DC power supply converts from 24V to 5V like the attached Webench report.
In their evaluation, LM2670 was not started up rarely when "Input" terminal is powered up from…
Part Number: LM2670 My customer is using the LM2670-adj to generate a 5.6V output from a 28V input. They notice that when they disable the device the output voltage momentarily jumps to ~9V, which is causing problems with downstream circuitry:
They…
Part Number: LM2670 Tool/software: WEBENCH® Design Tools Hi team,
Our customer inquired following issue.
I am using Power Architect in WEBENCH (Firefox with Flash plugin) and I want to setup the power tree for my PCB design using the LM2670 and…
Part Number: LM2670 Can the LM2670 use for a Li-Ion battery charger? The Technical Doc said under applications: Battery Chargers, but doesn't provide any example for battery charger circuit. I want to know if it will work for charging a Li-Ion battery…
Hello,
A simple question: In LM2670S (DDPAK Package) what potential is tab? For the same family switchers LM267x, (x = 3, 6, 8, 9) it is ground, but I have found nothing about 2670 and 2677 tab contact.
Regards