Part Number: LM2675 TI app note #SNVA538 has an equation on page 13 used to calculate the input impedance of a switching regulator circuit using the LM2675-5.0.
Ro = 5 ohm, Rl = 0.088 ohm, ESR = 0.09 ohm, D = 0.458, Lo = 68 uH, Co = 68 uF
I generated…
Part Number: LM2675 Hello technical support,
Could you help me to check the below picture of die and marking?
As show in below,one has a logo of national semiconductor and other dosen't.
How to understand the different logo?
I wonder if both are come…
Part Number: LM2675 Hello,
The absolute Max rating on LM2675's V SW pin is defined as -1 V (Max) as the parameter "Switch voltage to ground" in the data sheet. I guess this is a negative value, but what about a positive one? I don't think there is…
Part Number: LM2675 Other Parts Discussed in Thread: LM5010A , LM5010 , , LM5164
Hi Experts,
Our customer is looking for an alternative to Maxim MAX5035DUSA+. I found LM5010, LM5010A as an alternative to the MAX5035 but no direct option for MAX5035DUSA+ as…
Part Number: LM2675 Hi Team,
Good day! I need your help to check our customer's concern below.
TI has an application note #SNVA538 which explains how to properly design an input filter for a switching power supply using the LM2675N-5.0 as an example…
Part Number: LM2675 Other Parts Discussed in Thread: LM22675 , , LM2594 Greetings,
My customer is looking for a drop in replacement for the LM2675M-ADJ/NOPB they are using. I saw that the LM22675 is P2P, however is it ok to use without soldering the thermal…
Part Number: LM2675 Other Parts Discussed in Thread: LM2672 , Hi team
Could you help check if we have pin compatible device of LM2675MX-3.3/NOPB?
Vin: 36V Typ. 42V Max.
Vout: 3.3V
Iout: 500mA Max.
Let me know if you have any questions.