Part Number: LM2676 Other Parts Discussed in Thread: LM2679 Hi,
We use the LM2676-ADJ for the DC/DC buck from 24VDC to 8VDC, and now, we use the LM2679-ADJ with the same design, but the LM2679 has no output voltage, so please refer to below LM2676-ADJ…
Part Number: LM2679 Dear Expert of Power Design
We are using LM2679 to drive a TEC module, the resistance of the TEC is at the 1-ohm range, but not a consistent number, so we set the output voltage high, in the design is close to 10V. we use the current…
Part Number: LM2679 Hi,
We needed 12v from 24v supply so we are using the constant out LM2679SX-12 but when then inout voltage is slightly increasing let say 25/26 v the outpu is also increaseing from 12to16v can suggest any ideato rectifi
this. …
Part Number: LM2679 Hi,
For our internal project we are using LM2679SX-12/NOPB buck converter. Kindly review the attached schematics and let me know the comments if any.
Part Number: LM2679 Using LM2679T-12/NOPB, a circuit that outputs 24V input to 12V/5A was constructed. Measuring the output terminal measures 12V. However, when a load of 12V/1A is applied, only about 3V to 4V is output. What's wrong with my circuit?
Part Number: LM2679 Other Parts Discussed in Thread: LM2678 , LM2677
Hi Team, seek for some assistance.
LM2679SX-5.0/NOPB and it turns out that we may need to have an enable feature, which this part does not have. However, looking at the block diagram…
Part Number: LM2679 Other Parts Discussed in Thread: ASH , TPS2420
Hi all, Just finished the assembly of a few prototype boards and have encountered the following issue. While the circuit correctly outputs 7.4V ± 0.1V while not under load, when a 0…
Part Number: LM2679 Hello,
I am using the LM2679SX-ADJ/NOPB switching regulator in a pcb design and was experiencing a large voltage ripple on the output of the regulator that was about 500 mV pk-pk at ~750 Hz during a <100mA load. This was surprising…
Part Number: LM2679 I made a circuit that converts a 24V input to 12V/5A and tested it. However, when a load is applied, the output voltage drops to 4V. What's wrong with my circuit?
Below is the circuit I made, and I designed the circuit by referring…
Hello Lee,
I am sorry that this took so long. Here are a couple of things that should help:
It appears that the output capacitor is large for this converter. Please remove one of your output capacitors to see if stability is improved.
The…