Part Number: LM2679
Hi,
I am probably going to use LM2679SX-ADJ/NOPB regulator for my 7V project. Since i want to use TO-263 version, my only question which is not answered in the datesheet is where do i connect the TAB of this package? In datasheet…
Part Number: LM2679 Hi Team,
This is customer request and i would be very happy if you can support:
My customer currently working on EE: CNC control and they need support on DC/DC power supply.
The question is they used Webench for this design decided…
Part Number: LM2679 Hello
I have a project using DC-DC power converter to control LED with input voltage of 24 VDC and output voltage of 12V 2A. In this project, LM2679T-ADJ is used to adjust the output voltage.
However during the experiment, the maximum…
Part Number: LM2679 Other Parts Discussed in Thread: LM2673 , LMP8646 I'm trying to use the LM2679 Buck Converter to generate an adjustable negative voltage. My input voltage is 15 volts, and I was planning to use a potentiometer to adjust my output voltage…
Part Number: LM2679 Hi Team,
How much is the maximum voltage ratings of Current Adjust pin?
I understand the operation voltage of this pin is 1.2V(typ). However there is no definition of max voltage ratings on the datasheet.
Best Regards,
Koji Ha…
Part Number: LM2679 Other Parts Discussed in Thread: LM2671 Hi Team,
I have two question about the capacitor at output and Soft-start pin.
1.output capacitor
Can we use this device only the ceramic capacitor without the capacitor of large ESR for output…
Part Number: LM2679 Hi support team, About LM2679T-ADJ/NOPB,
Please let me know the Absolute Maximum Ratings of "Current adjust" terminal.
Regards, Dice-K
Hi,
Thank you for sharing this update. I am going to close this thread at this point. But please open a new thread or respond to this post once you get the new results!
Best Regards,
Katelyn
Part Number: LM2679 Other Parts Discussed in Thread: TINA-TI Tool/software: WEBENCH® Design Tools Hi!
I have a problem with Tina-TI Version 9.3.150.328 SF-TI with LM2679 Macro. In DC analysis while trying to get Nodal voltages calculated the program g…