Hi Viktorija,
To my knowledge, the pin-pin compatible device is LM2681 or LM2765, but their max load is 20mA. If the this is okay, then this can be considered as the 2nd source. Otherwise, I don't see another candidate.
Thanks,
Youhao
Hi Hollis,
I don't think this can be done by a single charge pump device. You need to consider cascading the charge pumps. The LM2682 is an inverting voltage doubler device. It can be used to generate -10V from a +5V rail, so you need first to produce…
And these National/TI charge pumps:
LM2765: http://www.ti.com/product/lm2765
LM2766: http://www.ti.com/product/lm2766
LM2767: http://www.ti.com/product/lm2767
Also LM2681 , LM2665.