Part Number: LM26LV-Q1 LM26LVCISD-135/NOPB, customer pn:136E5-S080070H-00
for this part the engineering team suggust have polar point for the marking. it will be central for the SMT mounting.
Part Number: LM26LV I'm designing a discrete 24volt high side switch circuit with Safe Operating Area (SOA) protection and fast current limit protection. The circuit uses a low RDS-on P-channel mosfet in a current limit configuration. That is, a sense…
Part Number: LM26LV Hello.
Is it safe to use the nOVERTEMP open drain output (pin 3) when the LM26LV is not powered? (Assuming the voltage at the nOVERTEMP pin is kept between -0.3 and 6V)
Also, is nOVERTEMP guaranteed to be high impedance to ground…
Part Number: LM26LV Hi everyone,
I'm considering to use this temperature sensor the code LM26LVCISD.
I was trying to find the power consumption in the datasheet but I can't find it. Does anyone know the power consumption of this temperature sensor…
Part Number: LM26LV The LM26LV data sheet suggests that all devices are designed for an operating range of -40°C..150°C (e.g. 6.4 Recommended Operating Conditions, 6.6 Electrical Characteristics). On the contrary chapter 12- Mechanical, Packaging, and…
Part Number: LM26LV Hello E2E,
If I ordering "LM26LVCISD-050/NOPB", how much the trip-temp and gain of this device? Can I have Explanatory material for suffix?
I want devices with trip points 42-deg and 45-deg.
Regards, ACGUY
Part Number: LM26LV Other Parts Discussed in Thread: TMP390 Hello,
I have a question about LM26LV.
My customer wants to order "LM26LVCISD- 042 /NOPB" and "LM26LVCISD- 045 /NOPB".
I checked LM26LV "Order Now" Page, but there are not above part numbers…
Part Number: LM26LV Hello,
My customer has a question about LM26LV.
[Q]
Is there a protective diode between the OVERTEMP * pin and the power supply to prevent ESD damage?
Is the same configuration as the following figure?
Best Regards, …
Part Number: LM26LV Hello
I plan to LM26L as a temperature sensor. looked over the DS , the gain 1-4 offers different temperature range. it is preset in factory. But how I can select the temperature range, basing on the marker, or model number.
…