Part Number: LM2733 Other Parts Discussed in Thread: TPS54060A , Tool/software: Hello everyone,
I have an 5V output from TPS54060A and I am using 5V to switch 12V with LM2733. You can see my design below. I am driving NCP81071B with 12V output and…
Part Number: LM2733 Other Parts Discussed in Thread: TLV61047 , Tool/software: Hi team,
Based on Figure 11, there are no information about the efficiency at less than 30mA or so. Does this mean this device can't work properly at the less than 30mA…
Part Number: LM2733 Tool/software: Hi Ti Experts,
We have here a case of 2 samples with same LM2733X device.
I would like to ask what the "ME" and "UK" die marking difference for the die marking below.
The die with "ME" marking has also 7.2A marking…
Part Number: LM2733 Tool/software: I'm looking for a boost converter to increase a single cell lithium 18650 battery voltage to 100V to drive a piezo ceramic transducer. The transducer will be toggled on and off with a low side FET at 40khz-150khz depending…
Part Number: LM2733 Other Parts Discussed in Thread: LM2735 Hello,
I have a question about LM2733.
I wonder how long will take time from input to output.
I can't find the information on spec. document.
Part Number: LM2733 Hello team,
My customer is considering to use LM2733 as constant current driver.
On the datasheet, LED current source is listed as the typical applications.
Is it possible to drive constant current with the configuration below…
Part Number: LM2733 Hi team,
Min input voltage is specified as 2.7V in the datasheet, but could you tell the device can work from what input voltage actually?
Customer uses battery as the input. And the input voltage can become lower than 2.7V because…
Part Number: LM2733 Other Parts Discussed in Thread: LM2731 , , LMR62014 Hi team,
The family device LM2731 is EOL, are there any plans for LM2733 to be EOL? I am considering LM2733 as a replacement for LMR62014, which is scheduled to be EOL, but I am…
Part Number: LM2733 Hi,
Would this be the correct connection to an MCU?
I would like the regulator to be active only when VDISPON goes high.
Regards,
Denny