Part Number: LM2735-Q1 Other Parts Discussed in Thread: TPS61040 , Hi Team,
May I know if have P2P option to replace LM2735XQMFX/NOPB? No need to change schematic and layout.
In customer usecase, input is 3.3V, output is 9V.
Thanks!
Ethan Wen
Part Number: LM2735-Q1 Other Parts Discussed in Thread: LM2735 LM2735YMFをつかってVin=5V、Vout=7VのDCDCコンバータ回路を試作しました。
Voutに負荷が無い状態では設計値通りのVout信号が得られますが、Voutに負荷がつながると
VinとVoutに大きなリプル電圧が現れます。回路図、基板パターン図を添付致します。
回路的に何か問題があるのでしょうか?見て頂ければ助かります。
また、基板パターン図は御社エバレー…
Part Number: LM2735-Q1 Hi Team,
Please help to review below schematic, customer reports that their LM2735Y with 520kHz application is being damaged in their design.
I checked with the design example and notice that the biggest difference is they did not…
Part Number: LM2735-Q1
Hello TI team
I need to do schematics review with your team
Input Voltage:5V
Output Voltage:10V
Output current:23mA
Fsw=520KHz
Can you please review the schematics whether components used are ok or not and also please do stabil…
Part Number: LM2735-Q1 Other Parts Discussed in Thread: TPS61378-Q1 , LM2735 Tool/software: WEBENCH® Design Tools I want to know what would be the inrush current at the startup based on Webench report?
Attached below is the Webench report
7571.12V 120mA…
Part Number: LM27313-Q1 Other Parts Discussed in Thread: LM27313 , , LM2733 , LMR64010 , LM2731 , LM2735-Q1 , LMR62014 Hello,
Currently we are using LM27313-Q1 for boosting an input of 5V to 6.2V. We are planning to use LM2733XMFX/NOP & LMR64010XMFX/NOP as an…
Other Parts Discussed in Thread: LM2735-Q1 Although it is not my work to review the data sheet of TI-components and it is not my aim to get more points by writing unnecessary stuffs.
but one my college is not happy with so many mistakes on data sheet of…
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LM2735-Q1 , LMR14030 , LM2735 Dear TI experts: The customer system has two levels of power. The first stage power supply is 12V to 3.3V, which supplies power to the system. The second stage power…
Other Parts Discussed in Thread: LM2735 , LM2733 , TPS61175 , TPS61170 Team,
Do we have other options to replace the SC4501 that seems to become EOL? https://www.businesswire.com/news/home/20060124005413/en/Semtech-Family-40V-2A-2MHz-Step-Up-DCDC The use case…
Other Parts Discussed in Thread: LM2735-Q1 , LMR64010 , LMR62421 , LM2735 , LM2731 , LM2733 , LMR62014 , LM3481-Q1 , LM3478 , LM3481 , TPS43061 , LM3488 I need to convert 5V DC to 19V DC with a maximum output current of 1 amp. The most important criterion I need…