Part Number: LM2776 I am using the LM2776 to supply the negative rail of a dual supply rail to rail in & out op amp. If the LM2776 has no output for the negative rail but the positive rail is still there, will the op amp swing to the positive rail or…
Part Number: LM2776 Hello
i have designed a negative 5V supply with the LM2776DBVR
as i read the datasheet i'm not sure what would be the best C FLY to chose ?
i chose 2 x 4.7uF ?
for the input / output i chose 10uF / 10uF (although the EVM has…
Part Number: LM2776 I am getting Vout = -0.7V for the LM2776 part with the following conditions:
Vin = 5.5V
C between pins 5 and 6 = 1 uF
Cout = 2.2 uF
Any clues what might be happening here?
Thanks,
John
Part Number: LM2776 Hello team,
The output ripple measurement graph (Fig 1) is very different from the output ripple calculation equation (equation 4) on the datasheet.
The shape of the graph on Figure 1 is not linear. What is the condition of the…
Part Number: LM2776 Other Parts Discussed in Thread: LM2663 , LM2662 Hi We can't find any stock of LM2776 in TI.com, is there any suggestion on the alternative TI parts we may consider? Thanks.
Part Number: LM2776 Other Parts Discussed in Thread: OPA2197 Hello everyone
Can I use two or more LM2776s by connecting them to the cascade? Not specified in its datasheet?
Part Number: LM2776 Other Parts Discussed in Thread: TPS60403 Hello
I have an appplication, that is sensitive to switching frequencies at about 10 bis 20 kHz. I uses the LM2667, which as a fundamentel switching frequency of 2MHz. In my application,…
Part Number: LM2776 Other Parts Discussed in Thread: TINA-TI Hi team,
We found a phenomenon in the process of applying LM2776, some doubts, would like to consult: When using LM2776 as a typical single-stage ChargePump application, through simulation…