Part Number: LM27761 Other Parts Discussed in Thread: LM2776 The datasheet says I can sim LM27761
webench.ti.com/.../quickview.jsp
The tool says part unsupported. Looking for +5 to -5 - Patrick
. 6765.lm27761.pdf
Part Number: LM27761 Hi Sir,
Could you support to provide output voltage ripple curve as following condition ?
1. Vin =3.6 ~ 5V ,Vout= -3.3V,Iout =5mA
2. Vin =3.6 ~ 5V ,Vout= -3.3V,Iout =100mA
2. Vin =3.6 V ,Vout= -3.3V,Iout =1/5/10/20/100/200mA…
Part Number: LM27761 Tool/software: Hi team,
Do you have newer alternative to LM27761, not need P2P, better 300mm wafer.
Input : 2.5~5.5V
Output : -5V
Load : 200mA
Thanks
Lillian
Part Number: LM27761 Tool/software: Hi Team,
I'm looking for rise time for the part : LM27761DSGT
Des: IC REG CHRG PUMP ADJ 250MA 8WSON
Trise or Ton =? to determine the power sequencing for the Digital display interface based application .
Regards…
Part Number: LM27761 Other Parts Discussed in Thread: DRV135 , , LM2776 Tool/software: Hi,
I’m currently building a board for an audio application, and I’m using the DRV135 line driver. It will be powered from +5 V and –5 V rails.
I need to generate…
Part Number: LM27761 Tool/software: Hi,
Our application uses a 12 V battery to power the RF section, which requires a low-noise –5 V supply capable of delivering up to 500 mA. Since this supply is intended for the RF section, the customer has specifically…
Part Number: LM27761 Tool/software: Dear Specialists,
My customer is considering LM27761 and has questions.
I would be grateful if you could advise.
---
I am considering using the LM27761 for generating -5V (10mA).
Q1: During startup and steady…
Part Number: LM27761 Other Parts Discussed in Thread: TPS63710 Hi Sir,
My customer want to find a low noise solution for their sensor application. (5V to -1.2V with LDO). Do you think we can use LM27761 for that? Or other suggestion? Thanks for your…
Part Number: LM27761 Tool/software: Hi,
I'm looking for some clarification on the startup characteristics of the LM27761. We are using this component in a design powered by a current restricted 5V5 supply (limited to about 40mA).
Do you have information…