Part Number: LM27762 Tool/software: The LM27762 datasheet Section 8.2.2 Detailed Design Procedure encourages you to use webench.ti.com/.../quickview.jsp WEBENCH fails to find it, even if you manually add the part number.
If you then try and report…
Part Number: LM25019 Other Parts Discussed in Thread: TPS61093 Tool/software: Hello all,
Please recommend the power supply solutions with the following parameters.
VIN=24V Iout_max=11mA
The output needs to be a ±15V power supply after isolation…
Part Number: LM27762 Tool/software: I would like to use a single supply analogue switch as part of a front end for a clock signal timing analyser. The key trait I am trying to create is a high fidelity representation of the clock signal zero crossing…
Part Number: LM27762 Tool/software: Hi everyone,
I'm using the LM27762 to generate dual rails of +3V and –2V, each supplying up to 100 mA. The input is a single-cell Li-ion battery, so the input voltage can range from about 4.2V down to something about…
Part Number: LM27762
I'm using the LM27762 to generate +5 and -5 voltages and I would like to use WEBENCH to simulate performance with various capacitors and resistors, as mentioned on page 13 of the datasheet. When I choose LM27762 in WEBENCH (webench…
Part Number: LM27762 Tool/software: Good morning,
I'm looking for a space qualified solution to generate a negative voltage supply. I have seen a few devices from TI that are capable of doing this but without SEP or SP part numbers.
Are there any…
Part Number: LM27762 Tool/software: My name is Oda. I purchased your LM27762 evaluation board and confirmed the behavior of PGOOD under negative voltage factor. According to P10 of the datasheet, it is stated that the PGOOD goes to “H” level when it reaches…
Part Number: LM27762 Tool/software: Hi,
I am trying to evaluate LM27762 design to generate +/- 5V from 5.2V input voltage.
I have observed that voltage at VFB- pin is out of spec.
Please find following design values
Vin = 5.2
For +ive voltage…
Part Number: LM27762 Tool/software: I would like to know about the setting range of the positive supply voltage. Is it possible to set it to be typ5V? (Is it possible to set it so that it could be 5.1V at max due to variations in resistors, etc.?)
Part Number: LM27762 Other Parts Discussed in Thread: TPS65131-Q1 Tool/software: Hi TIer
My customer need a charge pump with a +-6V output and a current greater and at least 150mA output as LCD power supply , do you have a recommendation?
I see…