Part Number: LM2903-Q1 Dear expert:
I have similar question. According to parameter Vicr and note3 of 6.6 EC table, can I draw conclusions listed below? Could you kindly correct me please?
1. common mode input voltage range is "0 to vcc-2v" at full range…
Part Number: LM2903-Q1 Hi team,
I would like to know the saturatoin voltage in our usecase.
Condition:
Vcc is +5V and +12V
Isink is 8mA
Tj is full range
Could you provide me with the data in our conditions?
I hope that it is less than 700mV.
Best…
Part Number: LM2903-Q1 dear expert:
i cannot understand Vicr on page5 of LM2903-Q1 datasheet. can you kindly correct me please?
1. does "0 to VCC-2" means that, both non-inverting input and inverting input should in the range of 0V to VCC-2V?…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: TINA-TI , Hello all,
Is it possible for LM2903-Q1 to operate when VCC=GND=0V and input differential voltage at IN+ or IN-? In the TINA-TI, it seems to output as normal operation when VCC=GND. Does…
Part Number: LM2903-Q1 Hi,
on the LM2903- Q1 , there is no max input current specified.
(the non-Q100 has a max of -50mA in the data sheet)
What is the max input current for negative input voltage?
Thank you
Cristian
Part Number: LM2903B-Q1 Other Parts Discussed in Thread: LM2903B , LM2903 , LM339 , TLV1812 Hi Staff
I have a question regarding the contents of the LM2903B-Q1 data sheet (SLCS141L).
A time summary of TR and TF is shown on page21 Response Time. • The rise…
Part Number: LM2903B-Q1 Other Parts Discussed in Thread: LM2903-Q1 , LM2903B Hi,
Could you please let me know the Quiescent current of LM2903-Q1? The LM2903-Q has 2-ch comparators and datasheet show as below.
Is the value for 2ch? I'm much confused because…
Davis,
This is an example of what I'm talking about:
Application Note: LM2903-Q1 Functional Safety FIT Rate, FMD and Pin FMA
Functional safety documents of some products can be obtained without a PPAP request.
Best regards, Shinichi Yokota
Part Number: DRV8718-Q1 Other Parts Discussed in Thread: LM2903-Q1 , Hi team!
The customer wanted to use DRV8718 VCP to supply for comparator LM2903-Q1. The VCP is about 22V and the comparator LM2903-Q1 electrical characteristics is as below. Is this acceptable…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903 Hi team,
We can see different LM2903 version in ti.com. In datasheet, there is no obvious difference for these parts. Could you kindly help comments on this so that my customer can place the…