Part Number: TLC2252A-Q1 Other Parts Discussed in Thread: LM2904-Q1 , OPA310 , TLV27L2-Q1 , LM2904B-Q1 Hello, are there (clamping) diodes between input and power supply in TLC2252A-Q1?
Because our vdd is not always powered, other circuits will be affected…
Part Number: LM2904-Q1 Other Parts Discussed in Thread: LM2904B-Q1
Hello,
Can you explain why it would be better to use the newly released LM2904B-Q1 in place of the older LM2904-Q1 version when selecting an amplifier for my automotive system designs…
Part Number: ALM2402-Q1 Other Parts Discussed in Thread: LM2904-Q1 , LM2903B-Q1 , LM2904 , LM2903B , LM2904B-Q1 Hello experts,
Hope you are doing well.
I would like to ask if the LM2904-q1 op amp has an internal clamping diode. In customer's test, when the…
The TS321-Q1 has exactly the same characteristics as the LM2904-Q1. But there is no -B model.
The TL971-Q1 does not have rail-to-rail inputs. If you are using input voltages near −5 V, use the TLV9151-Q1 or TLV9351-Q1.
Part Number: LM2904B-Q1 Other Parts Discussed in Thread: LM2904 , LM2904B , LM2904BA Dear team,
What does ”device marketing“ mean? What is the difference between these device besides different package type? I can't search for example 2904AVQ or…
Part Number: LM2904B-Q1 Other Parts Discussed in Thread: LM2904-N , LM2904 , LM2904B Hi team,
I have a question on the maximum allowed current through the internal ESD diode structure, in case the IC is unpowered?
Thanks and best regards,
Michael
Part Number: LM2904-Q1 Other Parts Discussed in Thread: LM2904-N Hi team
My customer asked input current of Absolute maximum ratings.
For the LM2907, the Absolute maximum input current displays 50mA as shown below.
But, I don't find Absolute maximum…
Part Number: LM2904-Q1 Other Parts Discussed in Thread: TLV313-Q1 , TLV3011 , TLV3012-Q1 Hi team,
Could you please help to check if we have automotive qualified opamp to replace SGM321YC5 and SGM8710? Better to have P2P solution.
Thanks!
Part Number: LM2904-Q1 Other Parts Discussed in Thread: LM2904 Hi team
Low Supply-Current Drain Independent of Supply Voltage . . . 0.7 mA Typ
Above is the specification of the consumption current. I want to know the standby current when 16V is applied…