Part Number: LM2936
Hello,
I am designing circuit that is used LM2936HVBMAX5.0/NOPB.
I would like to confirm that LM2936HVBMAX5.0/NOPB has SD pin (5pin).
Let me check it just in case to avoid making mistake in my design.
Regards,
MESH
Part Number: LM2936 Other Parts Discussed in Thread: TPS7A16 Hello E2E,
What is the quiescent current at 48Vin?
Its d/s only show the quiescent current at 40Vin,max.
~Jason
Part Number: LM2936 Hello.
Could you please specify the document, which describes differences between two versions of LM2936 LDO: LM2936M-5.0/NOPB vs LM2936M-5.0.
In our device we used LM2936M-5.0. What the risks have we to take into account if we…
Part Number: LM2936 Hi,
There is a min value of 22uF for stability in the datasheet of the 3.3V version. Is that a "one size fits all" constraint or are there other conditions for stability using a 10uF capacitance ?
My application has a 3mA current…
Part Number: LM2936 Other Parts Discussed in Thread: DRV8313EVM , , DRV8313 The data sheet for this part on Page 15, paragraph 8.2.2.2 spec's that the output cap needs to be tantalum (based on requirements) but it goes on to say a ceramic MLCC can be…
Part Number: LM2936 I purchased several fixed output LDO regulators, specifically LM2936Z-5.0/NOPB.
I connected this LDO with a 100nF capacitor on input and a 100uF cap on the output as the datasheet shows. With a 12-20V input the output is at 5.0V…
Part Number: LM2936 Hello,
Datasheet item 6.1 Absolute Maximum Ratings note (3) states de following:
" The maximum power dissipation is a function of TJ(MAX), RθJA, and TA. The maximum allowable power dissipation at any ambient temperature is PD …
Part Number: LM2936 Other Parts Discussed in Thread: TPS7A16 Operation of LM2936Z with input above 40V.
We've got a board that uses the LM2936Z-3.3 device, and need it to operate with an unsmoothed rectified supply that goes to about 46V peak. The High…
Part Number: LM2936 Dear all,
can you suggest a circuit to generate a delayed power on using the SD pin ? The LM2936 has a SD which works in the opposite way respect with most of similar devices.
regards,
Domenico