Part Number: LM2936Q-Q1 Hello,
I am currently reviewing the following orderable part numbers:
LM2936QMP-5.0/NOPB
LM2936QMPX-5. 0 /NOPB
Based on the information available in the datasheet, both devices appear to be identical in terms of electrical…
Part Number: LM2936Q-Q1 Tool/software: Hi,
are the NC pins of this device really not connected inside the device? Is it possilble to connect them to Vout without any impact?
My customer wants to replace another device.
Best regards
Part Number: LM2936Q-Q1 Dear partner,
For this MPN LM2936QM-5.0/NOPB, d ifferent bottom mold marks were observed, one with "M" while the other one without "M".
Could you please give an explanation about the variation?
Thank you so much for your…
Part Number: LM2936Q-Q1 Hi,
Good Day.
I need some information about PIN 5 of the device. The pin is left floating on the PCB and on the datasheet is written that to have the device on is possible to leave the pin floating (open). In the datasheet…
Part Number: LM2936Q-Q1 Hi Team,
I needed your help in clarifying conflicting information that I found in the datasheet for this device.
(1) In section 6.3, and 7.3.1, the recommended operating condition for LM2936Q is 40V and 60V max for LM2936QH…
Part Number: LM2936Q-Q1 Other Parts Discussed in Thread: TPS7B81-Q1 , TL720M05-Q1
Hey Team,
I am looking at moving from the LM2936Q-Q1 to the TPS7B81-Q1 . Both packages would be TO-252, however the LM2936Q-Q1 is a 3-pin package and the other is 5…
Part Number: LM2936Q-Q1 Hello ,
As per Datasheet , Quiescent current is provided for load of 10mA and 50mA.
Our requirement is for load current of 20mA. Can you provide value and graph for quiescent current at 20mA?
ASAP.
Thanks,
Gaurav
Part Number: LM2936Q-Q1 Hi team,
What is the difference between LM2936QHBMA-5.0/NOPB and LM2936QM-5.0/NOPB? It looks like they are both SOIC-8 and in tube, but they have different cost.
Thanks,
Connie
Part Number: LM2936Q-Q1 Other Parts Discussed in Thread: LM2936 Hi Team,
My customer(Hitachi) is considering to use this device.
But they are concerned how long start-up time is.
Need the typical value soon.
Regards,
ti
Hi Ajay,
Unfortunately, I'm unable to share the source datasheet, only the curve itself. A link to the image file is here: pastedimage1753218929606v1.png (580×414)
New chip TLE4275-Q1 devices have an absolute maximum Vin rating of 40V, while legacy…