Part Number: LM3150 Other Parts Discussed in Thread: CSD18513Q5A , CSD18563Q5A We are currently using the LM3150 to convert 24 V to 5 V and a seconden one for 24 V to 12 V. Normaly we are using the CSD18563Q5A as MOSFET 1 and 2. Unfortently this MOSFET…
Part Number: LM3150 Other Parts Discussed in Thread: CSD18563Q5A , LM25145 Hi,
I am uisng LM3150 , so far it is good. But I am curious one thing for chip temperature.
Test setting is: 24V input, wihout loading, with the different output voltage.
The question…
Part Number: LM3150 Other Parts Discussed in Thread: LM25145 , LM5146 , LM5145 , LM25148 I am uisng LM3150 , so far it is good. But I am curious one thing,
My understanding, LM3150 max drive current shoud b e decided by MOSFET, and sample res ? But in the datasheet…
Part Number: LM3150 Other Parts Discussed in Thread: LM5160 Hi TI Teams.
①Is it possible to use LM3150 as a Fly-buck?
The primary output is 3.3V/1.5A, second side output is 5V/100mA,±15V/150mA.
②I understand that the requirement for the fly-buck…
Part Number: LM3150 Other Parts Discussed in Thread: LM34922 , Actually i wanted to use the LM34922 in current mode for this design, but since this device ist not available anywhere, i did the design with the LM3150, because of the fast transient response…
Part Number: LM3150 Other Parts Discussed in Thread: LM25145 Hi,
In LM3150, How to set switching frequency ? and due to COT architecture , If input voltage and Load varies whether it will vary switching frequency.
Part Number: LM3150 Hi,
I tried to implement a LM3150 from the webench simulator. 8103.WBDesign19.pdf
after killing 10xLM3150 i gave up. I had two PCB working temporary mod_19v_revB.zip the LM3150 was getting always hot and where doing a peeping noise and…
Part Number: LM3150-500EVAL Other Parts Discussed in Thread: CSD16342Q5A , LM25145 , LM3150 , LM25149 , LM25148 , LM5146 , LM5145 , LM63460-Q1 Hi TI,
I'm going to use this convertor in my PCB board for below mentioned configuration,
Vin = 12 V to 20 V
Iout…
Part Number: LM3150 Hi experts!
Just curious, why is there an "RonD" included in the section 9.2.2.3 of the datasheet?:
I notice if I follow equation (4) of the datasheet using passive values from the 250KHz eval board, I calculate Fsw =…
Part Number: LM3150 Other Parts Discussed in Thread: LM5145 Hi team,
My customer want to know, do we have Safety certificate and test report on this device.
If we have, could you provide to me, thanks.