Part Number: LM317 Tool/software: Dear all, Currently I have a project to build a simple power supply with 8 channels isolated. The requirements are the output needs to be 4V fixed with a ripple less than 2mV (1mV will be great) and the output current…
Part Number: LM317 Tool/software: Hii team,
I am using LM317DCY (U21,U18) as regulator to convert from 24-15 and 15-7 but output voltages are not as expected ... Check the implemented circuit below for reference.
Part Number: LM317 Tool/software: hi,
for LM317SX/NOPB, customer has some inventory and want to prebake but their equipment only supports up to 98℃.
datasheet states 125℃/48h but how long should they bake at 98℃? or is 125℃ a necessary requirement?
regard…
Hi Ishaan,
Here's an overview of the test setup.
Basically the LM317 supplies current into the circuit. The comms interface in the master (and similarly in slaves), use transistor Q6 to either pass current (i.e. the idle-line "mark" state) or turn…
Part Number: LM317 Tool/software: Need to have a reference circuit for using LM317 as constant current of 1mA.
application - will be use to sense temperature from PT100 sensor. (3 wire)
Voltage used is AA battery - 3V.
Part Number: LM317 Tool/software: Hi team,
My customer designed LM317 in their system but seems thermal problem, so they consider to use 3pcs devices to share thermal.
Can they just do parallel design? Or any circuit we need to modify?
Part Number: LM317 Tool/software: I understand the normal equation will be below.
However we saw on the specification this formula adding R3 and -10V in the mix.
May I know when we will use both formula and what is the model behind the second equation…
Part Number: LM317 Tool/software: dears,
My customer is seeking for 35V vin, 1.5A output LDO, LM317KTTR may meet these requirement, but their environment temp range is -40~125 degree C? could LM317KTTR may be able to support this case?
if any other TO-263…
Part Number: LM317 Tool/software:
dears,
My customer is seeking for 35V vin, 1.5A output LDO, LM317KTTR may meet these requirement, but their environment temp range is -40~15 degree C? could LM317KTTR may be able to support this case?
if any other TO-263…