Part Number: LM317-N Hi support team, In the Typical Application item on the first page of the data sheet, About C1 (input capacitor).
* Needed if device is more than 6 inches from filter capacitors.
Should I place the C1 if the current is small (eg 30mA…
Part Number: LM317 The LM317EMP has an ESD voltage rating of 3000V. The MIL-STD-461 CS106 test is approximately a 400V sinx/x for 5usec. The human body model decays quickly in under 500nsec. The CS106 at 5usec has >10x Joules the Human Body model. Do…
Hi OMG,
The layout looks fine.
Here's what I'm thinking. The junction temperature for the LM317-N, from your measurement, is estimated to be 76C + 2W * 10.4C/W = 97C, and if your board was similar in thermal performance to the JEDEC High-k board from…
Part Number: LM317-N Hi team,
My customer is considering to use LM317EMP/NOPB. I think that this device allow ceramic capacitor. Is my understanding correct?
Cin : 1uF Ceramic capacitor
Cout : 4.7uF Ceramic capacitor
Vin : 12V
Vout : 7.5V (R1=240ohm, R2…
Other Parts Discussed in Thread: LM317-N , TPA6120A2 , TPS7A33 24V input, two LM317-N can output -12V?
I want to drive the earphone with tpa6120a2, its power supply needs =-12V,
So, is there a reference circuit?
Part Number: LM2940-N Other Parts Discussed in Thread: TPS7A47 , TPS7B86-Q1 , LM317 Tool/software: Hello, I am currentling using LM2940T-5 for my design.How can I increase the output voltage by 200 mv? I tried using a resistive divider connected between…
Part Number: LM317-N Other Parts Discussed in Thread: LM317 Can someone help me to get the updated 197 SVHC reach statement for the texas instrument component LM317T/NOPB??
In advance thank you for your help and support.
Best Regards.
Gabriel
Part Number: UC1825 Tool/software: Hi team,
I think there is Potential device class (M, Q, V, B, T, N) in MIL-PRF-38535, but the Device Marking for UC1825L883B is 5962-87681012A, so is class M correct?
Thanks
Best regards,
Masahiro Kobayashi