Part Number: LM317L Tool/software: Hello Support Team,
I have the following circuit:
My Problem is that I get a large transient on the output when I switch on the Vin (24V). I'm using a toggle switch.
Blue = Vin
Yellow = Vout
The output…
Part Number: LM317L Tool/software: Hello,
we use the LM317LITP component (DSBGA (YPB) with 6 pins). The first samples have been manufactured, but unfortunately, there are problems with the component's soldering. Under slight mechanical stress, the balls…
Part Number: LM317L Tool/software: Hello, Could you share with us the ESD (HBM and CDM ) information for the LM317L, LM2676S, LM79L12ACM and LM317LM/NOPB? Information is not available in datashee
Part Number: LM317L Tool/software: Hello TI Team,
Please confirm if Plexus PO# 717-13822027-OP is affected by PCN# 20250115000.1 (Qualification of FFAB using qualified Process Technology, Die Revision and Datasheet update for select devices) ?
Part Number: LM317L Tool/software: Hi Team,
I have 2 questions about this component. - LM317LIDR
In case that I adjust the Vout to be 24V and the Vin is less than 24V+2.5V (Input-to-Output voltage differential is less than the recommended –…
Part Number: LM317L Other Parts Discussed in Thread: LM337L , LM317 , LM337-N Tool/software: Hi,
I am using TI's LM317L, LM337L, and TPS76350DBVR LDOs in my daughtercard transformer circuit to provide various output voltages; e.g. +/-12V and +5V. What…
Part Number: LM317L Tool/software: Hi team,
Are the characteristics of the new chip as follows?
- A minimum load current of 5mA is required - If Vin-Vout is large, only 25mA can be output
Despite this, the load conditions are the same for Legacy…
Part Number: LM317L Tool/software: Hi Staff
I have a question regarding LM317L datasheet (SKCS144F) 5.5 Electrical Characteristics "Peak output current". The TEST CONDITIONS for [Peak output current] says "3V ≤ VI - Vo ≤ 13V".
Separately, the 9 Revision…
Part Number: LM317MQ Other Parts Discussed in Thread: LM317L Tool/software: Hi team
Would you help double check if LM317MQ also support Constant-Current, Battery-Charger Circuit like LM317L?
LM317L is used as a NiH battery charger function in my…
Part Number: LM317L-N Tool/software: I am using a Japanese translation software. Thank you for your question.
I am using resistors R1 = 240Ω and R2 = 2kΩ (resistor connected between the adj terminal and GND) so that the input voltage is 15V and the…