Other Parts Discussed in Thread: LM324-N Dear TI engineer.
I have a few questions.
1. If the surface temperature of the LM324N of 61 ℃ (@ ambient temperature of 24 ℃), can I see that the LM324-N is normal behavior?
2. Do you have a guide that will be sure…
Other Parts Discussed in Thread: LM324-N , LM324 Dear TI engineer.
I have a few questions.
1. If the surface temperature of the LM324N of 61 ℃ (@ ambient temperature of 24 ℃), can I see that the LM324-N is normal behavior?
2. Do you have a guide that will…
Part Number: LF347-N Other Parts Discussed in Thread: LF347 , LM324 , TL3474 We are replacing obsolete part MC34074P with the pin for pin TI part LF347N/NOPB in the attached circuit. Are there different operational amplifier formulas available to control…
The diode is not designed to carry large currents, so its forward voltage might increase quickly.
A different die indeed might change the diode, but not the characteristics of the opamp itself. (But are you sure you didn't look at a different device like…
In My circuit I am using LM324 and P and N Channel Mosfet to generate 0-20mA. But some of our customer looking for 0-1V or 0-10V output which I am trying to use multiplexer with some resistors.
Thank you
Curtis,
Did the new batch of boards fail after a 15kV ESD test?
LM324N and LM324AN do not share the same silicon die. There will be subtle differences, but both are compliant to the data sheet parameters.
LM324-N (this 'N' represents National Semiconductor…
Part Number: LM358LV Other Parts Discussed in Thread: LM358B , LM358-N , , LM358 , LM324 , LM321LV , LM324LV , LM321
Hello,
When searching for an LM358 I found a bunch of different versions, LM358, LM358-N, LM358B, and LM358LV.
What's the difference between…
Andy,
TS321 is the single version of LM324 or LM358. LM321 is the single version of LM324-N or LM358-N
These facts are not obvious therefore, Paul did not know this.
Tseng,
I understand better now. I will simulate a filter on Monday.
Is the distortion you have now servere (visible on oscilloscope waveform) or slightly higher THD+N?
If LM324 output has to change between sourcing and sinking output drivers, then there…