Part Number: LM324A Other Parts Discussed in Thread: LM2902 , LM124 , LM2902BA , LM324BA , , LM2902B , LM324B I have a legacy design using LM324APW (TSSOP pkg) that I'm adding alternate parts to the BOM. What are the drop-in compatible part numbers? There…
Part Number: LM324A Hello TI team,
In our existing design we are using "LM324APWR" IC part.
Now, we want to replace "LM324APWR" by "LM324APWRG4" IC part.
Can you please support me to answer below queries,
1. What is the main…
Part Number: LM324A Other Parts Discussed in Thread: LM324 , LM324-N
Hi Guys,
I need your help. We are having some trouble with the op-amp, negative input going low impedance and I’m don’t know why this might be happening.
The circuit is shown…
Part Number: LM324A Other Parts Discussed in Thread: LM324 , LM2902B , TINA-TI Hi, I admit that I am exceptionally new to LTSpice, but while attempting to simulate the op amp LM324 on LTSpice, I was unsuccessful in getting the op amp to simulate even when…
Part Number: LM324 Dear TI support team;
When using the same circuit, the output of LM324 is smaller than that of LM324A. I download the specification and see that the two are the same.
Can you tell me the difference between the two?
Thanks a lot…
Part Number: LM324A Other Parts Discussed in Thread: LM324 , LM2902K , LM324K , LM358 Hi Support team
May I know the Vf of Internal clamping diode
thank you
Hello Shivangi,
The output range of LM324 is about 0V to 1.8V at 25C and less range at -40C. If sinking much output current then things get worse.
The output range of LM324A is better, 0V to 3.3V
For both, the valid input common mode range doesn't go…
Part Number: LM324A Hi Support Team,
My customer wants to know what is the negative voltage clamping rating for input clamping diode? Is it -0.3V as datasheet specified?
In their application the input voltage would go lower than -0.3V for around 5…
Part Number: LM324A Other Parts Discussed in Thread: LM324-N , LM324 , LM2902KAV , LM2902K , LM324K , LM2902 I have an old PCB that I am updating so that it will pass the 15kV air discharge test. It is using the LM324N, and LM324AN interchangeably as voltage…