Part Number: LM334 Other Parts Discussed in Thread: LM234 , , LM134 Hi,
We need a small constant current source of about 50 uA. The available compliance voltage is about 1.2 V.
My understanding is that LM134/LM234/LM334 is suitable because it can…
Part Number: LM334 Tool/software: Hello,
We are using an LM334 device in our circuit configured as a constant current source of 35uA. The resistors used to set the current are 0.1% tolerance. We have built and tested a batch of 31 circuits and measured…
Part Number: LM334 Other Parts Discussed in Thread: TLA431 Tool/software: Hello All,
I'm building a gang charger station for supercaps (HLC). The current is limited to 5mA with an LM334.
I had to limit the final charging voltage to 3,6V. Using a…
Part Number: LM134 Other Parts Discussed in Thread: REF102 , REF70 , REF54
Tool/software:
Hi,
I want a very stable precision current source for JFET tail biasing. The current source should have a positive temperature coefficient to cancel out…
Part Number: LM334 I am trying to use an LM334 to supply 2.1mA to a capacitive load and I get some large spikes in the voltage. I've reduced my circuit down to what is shown The signal acquired is AC coupled to eliminate the DC offset, but R1 has about…
Part Number: LM334 Other Parts Discussed in Thread: ATL431LI Hi team,
I want to use simulation software to achieve that 10mA Constant Current Source with LM334. Do we have emulated software that can do this?