Part Number: LM337 Other Parts Discussed in Thread: , TPS7A33 Tool/software: Hi Team,
What's the difference between LM337 and LM337-N? Thanks in advance.
BRs,
Francis
Part Number: LM337-N Tool/software: Dear Sir/Madam,
We hope this message finds you well.
We have received an inquiry from our customer regarding the RoHS exemption for LM337T/NOPB.
Currently, the LM337T/NOPB falls under the EU exemption code 7(a…
Part Number: LM337-N Hi all,
I would like to know the difference between θjc.
LM337T/NOPW as an alternative to LM337KCS, the value of θjc is very different.
LM337KCS : 3℃/W
LM337T/NOPW : 15.7 ℃/W
What is the difference?
Is it because the…
Part Number: LM337-N-MIL In our Amplifier application, the Voltage regulator of LM337H/NOPB is touching the metal lid of the body casing, it then causes the failure: short circuit between this voltage regulator LM337H/NOPB and the lid body casing. It…
Part Number: LM337-N We are using LM337N to generate -8V from -15V. When the load current of the LM337N increases and its heat is generated, there are individuals where the output voltage ripple increases and individuals where it does not. -1 What is…
Part Number: LM337-N Hello, dear colleague. We have product LM337IMP/NOPB. There is marking on top: 8777, N02A. The service of warehousing needs information about the date of production of the product, please give these data. Thanks for your help. email…
Is the metal body of the voltage regulator LM337H/NOPB may cause the short circuit if it touches with other components/metal components? Because, from our understanding, the body of the component should be inductive, and not conductive. Can you please…
Part Number: LM337-N Other Parts Discussed in Thread: LM337 , LM317 hello,
I work with this component in its normal configuration (Figure 1), and according to the resistor ratio, I should be at the output -49Volt.
when I work with the regulator…
Richard,
The info in the abs max table and recommended operating conditions table in the datasheet for LM337-N is correct and has always been correct. There may have been a mistake in the ordering table at the end of the datasheet which has been fixed…
Part Number: LM337-N Other Parts Discussed in Thread: LM337 , LM317 , LM317-N
I am using an LM337-N in sot-223 package. The circuit is simple, but I find the output of the circuit is ringing at a frequency about 17kHz. (I am sorry I have put a wrong…