Part Number: LM337-N Tool/software: Dear Sir/Madam,
We hope this message finds you well.
We have received an inquiry from our customer regarding the RoHS exemption for LM337T/NOPB.
Currently, the LM337T/NOPB falls under the EU exemption code 7(a).
We…
Part Number: LM337 Other Parts Discussed in Thread: , TPS7A33 Tool/software: Hi Team,
What's the difference between LM337 and LM337-N? Thanks in advance.
BRs,
Francis
Part Number: LM337-N Hi all,
I would like to know the difference between θjc.
LM337T/NOPW as an alternative to LM337KCS, the value of θjc is very different.
LM337KCS : 3℃/W
LM337T/NOPW : 15.7 ℃/W
What is the difference?
Is it because the die…
Part Number: LM337-N-MIL In our Amplifier application, the Voltage regulator of LM337H/NOPB is touching the metal lid of the body casing, it then causes the failure: short circuit between this voltage regulator LM337H/NOPB and the lid body casing. It results…
Is the metal body of the voltage regulator LM337H/NOPB may cause the short circuit if it touches with other components/metal components? Because, from our understanding, the body of the component should be inductive, and not conductive. Can you please check…
Part Number: LM337-N We are using LM337N to generate -8V from -15V. When the load current of the LM337N increases and its heat is generated, there are individuals where the output voltage ripple increases and individuals where it does not. -1 What is the…
Part Number: LM337-N Hello, dear colleague. We have product LM337IMP/NOPB. There is marking on top: 8777, N02A. The service of warehousing needs information about the date of production of the product, please give these data. Thanks for your help. email post…
Part Number: LM337-N Other Parts Discussed in Thread: LM337 , LM317 hello,
I work with this component in its normal configuration (Figure 1), and according to the resistor ratio, I should be at the output -49Volt.
when I work with the regulator stand-alone…
Haiyong,
LM337IMPX/NOPB would be your best option here in Adjustable version.
https://www.ti.com/product/LM337-N/part-details/LM337IMPX/NOPB
Regards,
Prakash L
Richard,
The info in the abs max table and recommended operating conditions table in the datasheet for LM337-N is correct and has always been correct. There may have been a mistake in the ordering table at the end of the datasheet which has been fixed…