The LM337 only has 2 models and neither link provides a TSM file upon download (not even CIR/LIB/MOD) even when I try using the New Macro Wizard it doesnt seem to find it. I'm looking specifically at the "LM337-N Unencrypted PSpice Transient Model" link…
Part Number: LM2940C Other Parts Discussed in Thread: LM2990 , LM79 , LM337-N Hi all,
Can LM2940C be used for Negative voltage?
Because LM2990 is too much High-cost. My customer rejected it.
If you have the idea for negative voltage use, please teach me the…
Part Number: TPS7A33 Other Parts Discussed in Thread: LM337 , , TPS7A39 , LM2991 , UCC284 , LM337-N , LM237 Hi team,
do we have anything similar to the LT3081-LT3091?
Other than the TPS7A33/53 and the LM337 family, do we have anything else that has negative…
Scott,
The LM337IMP is a LM337-N device.
To be clear, there is an LM337-N device and an LM337 device on ti.com.
This is due to the acquisition of National semiconductor. The LM337-N device is the old National version of the device, whereas the LM337…
Hi Dave,
There is also the LM337-N that comes in a SOT23 that should also suit your application. This part says that it can be ordered through a distributor.
Regards,
Mark
Other Parts Discussed in Thread: LM317-N , LM337-N Does the architecture below work with LM78L15? Application is actually +24V source and they need +/- 15V for an OPAMP. Any other devices that should be considered?
Other Parts Discussed in Thread: LM1084 , LM317-N , LM337-N , LM1086 , LM340 Hello,
We have two inputs: +15V, -15V and a common, we need to use two LM1084 to generate +12, -12V and a common. Could we connect the two LM1084: U1, U2 in the following:
1) Input…