Part Number: LM337L Other Parts Discussed in Thread: LM337
I am having analog voltage in the range 0-10V or analog current in the range of 4-20mA, either of them entering a same 2 position connector (here a 5 position connector, kindly neglect it).…
Part Number: LM337L Other Parts Discussed in Thread: TPS7A33
Whether LM337L can meet the following conditions: input voltage -15V output -12V, output peak current 173mA, average current 130mA; .
Thanks
Part Number: LM337L Other Parts Discussed in Thread: TPS7A3401 , LM337 , TPS7A30 Hello,
i want to use the Webench design tool to create a negative switching regulator circuit. Unfortunately, the device cannot be called up with the Webench tool. Can…
Part Number: LM337L
Hello Team,
My customer would like to know the Power Dissipation (Max/Typ) For this Part LM337LZ/NOPB. I can't find this in the datasheet.
Regards,
Renan
Part Number: LM337L Hi team.
Our customer wants to use this device with ceramic capacitors for area saving.
So they want the data of ESR requirement for device stability.
Do you have any data like that we can understand ESR stable region?
best…
Part Number: LM337L Other Parts Discussed in Thread: LM317L Hi team,
my customer wants to know specs which cannot be found in datasheet. If it's available, please provide?
1. accuracy over the full temperature range (-25∽125 °C):
2. temperature…
Part Number: LM337L
Hi,
Is the LM337LZ / NOPB produced in 2012 compatible with RoHS10?
Since the data sheet contains only current information, please tell us the past information.
I would like to confirm that there is no difference from recent…
Part Number: LM337L Other Parts Discussed in Thread: TPS7A30 Hello Team,
I have 3 inquiries about LM337L
My customer considers to use it with VIN-VOUT condition = around 2V.
(1) I cannot find "Vin-Vout" condition in recommended operating condition…
Part Number: LM337L Other Parts Discussed in Thread: TPS7A30 , , LM337 Hello team,
I have a question about LM337LM/NOPB.
Is there any data or useful information for dropout voltage vs. temperature?
Best regards,
Part Number: LM337L Hi all Would you mind if we ask LM337L? Our customer tries to use follow conditions; -120ohm / 560ohm Vout=-7V -1.2kohm / 5.6kohm Vout=-7V On the datasheet P1, the resistance value is R1=240ohm and R2=ADJ. So, in case of kohm unit…