Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LM337L Other Parts Discussed in Thread: LM337 Dear LDO Team,
LM337 has some descrepancies on temperature information on the datasheet: on recommended op conditions it is mentioned -25-125C whereas on orderable is downto 100C max and for LM337LZ…
Part Number: LM337L Hi all Would you mind if we ask LM337L? Our customer tries to use follow conditions; -120ohm / 560ohm Vout=-7V -1.2kohm / 5.6kohm Vout=-7V On the datasheet P1, the resistance value is R1=240ohm and R2=ADJ. So, in case of kohm unit, if there…
Part Number: LM337L Hi E2E,
Good Day!
Looking at the datasheet of LM337L, http://www.ti.com/lit/ds/symlink/lm337l.pdf
There's a discrepancy on the pinouts of TO-92 package when you check page 1 and page 20. Below are the images captured from the same…
Part Number: LM337 Other Parts Discussed in Thread: , LM317 , TPS7A39
I am designing a bipolar power supply circuit using LM317lL and LM337L. I started out using LM337N in PSPICE for TI because LM337L is not available. Ultimately I will need LM337L for…
Part Number: LM337L Other Parts Discussed in Thread: LM337-N , Hi,
a costumer of mine would like to know how the ripple rejection of the LM337L perofrmes over frequency. In the datasheet of the LM337-N are plots that show this info. Do we have such plots…
Part Number: LM337L Other Parts Discussed in Thread: LM337 Hi,
My customer has the following questions:
For the LM337 for 3.3 V output < 100mA load application:
1- Could ceramic capacitor of 10uF OK for the design on the output regulator for output…
Part Number: LM337L Other Parts Discussed in Thread: LM337 Hi Support team,
Could you give me the following the customer question?
<Customer question>
At LM337L datasheet p7 at Figure 5, C2 is mounted. What is the purpose to mount C2 on LM337L circuit…
Part Number: LM337L Hi team,
Could you tell me the minimum input voltage for turning on? I didn't find UVLO or something like that at the datasheet. Thank you for your support.
Best regards,
Takeshi Sasaki
Part Number: UA78L Other Parts Discussed in Thread: LM317L , LM337L , I want to ask about how to calculate the thermal performance of these three devices.
My operating condition is shown below:
(1) UA78L05, from 15V to 5V at 0.1A under 105 degree of ambient…
Part Number: LM337 Other Parts Discussed in Thread: , TPS7A39 , , LM317
I am trying to add current limiting to the previously submitted design by adding LM317 and LM337 regulators in current-limiting mode. Both simulate nicely standalone but don't deliver…