Part Number: LM339B Other Parts Discussed in Thread: LM339 Hi Amplifiers team, I have an engineer asking about the current limit of the LM339BIPWR hwne the voltage at the IN- pin is greatere tan the V+ pin (V- = GND)?
The existing design uses 150k current…
Part Number: LM339B Other Parts Discussed in Thread: LM339 Hello,
Can the LM339BIRTER operate with its DAP/thermal pad floating?
I have a prototype build where I use the LM339BIRTER. Unfortunately, due to a PCB layout SNAFU, the DAP ended up connected…
Part Number: LM339B Tool/software: LM339BIDR is Wave Soldering Compatibility?
If you are able to accommodate, please let me know the conditions.
Please tell me the maximum soldering temperature and time.
Part Number: LM339B
Tool/software:
Hi team,
When using the LT Spice model of LM339B with one of the inputs outside of the Vcm range, the simulation is not outputting a clear ON nor OFF, but is outputting some voltage between low and high. Datasheet…
Part Number: LM339B Hi All,
Customer is considering LM339B. I am concerned about whether it is resistant to static electricity. Therefore, I am wondering whether to install an additional protection diode. Installing protection diodes increases costs…
Part Number: LM339B Other Parts Discussed in Thread: LM393B , LM339 Hello team,
I have a quick question.
Is the input voltage under the ABS max allowed to be biased regardless of the supply voltage condition for LM339B and LM393B? (e.g. Vin=32V with…
Part Number: LM339B Hi,
I need an OR function on 2 of my outpust from LM339BIPWR. Can I connect them together on the output to get an OR function without any diodes connected to the outputs?
Best regards, Kenneth
Part Number: LM339B Other Parts Discussed in Thread: LM339 Hi,
Chen tieing the 2 output ports together, I get only 1.5V on the output if only one of the inputs are high. When high on both inputs the output is 5V. Previously I was told I could just tie…