Part Number: LM2901 Other Parts Discussed in Thread: LM339LV , Hi,
The customer finds a problem. When LM2901DR is supplied with 3.3V power, the output fails under -10 ° C in a low temperature environment. The waveform is as below, and the output failed…
Part Number: LM2901AV Other Parts Discussed in Thread: LM339LV , LM2901 Hi Expert,
I have a question about the transition state of LM2901AVQPWR. The following is the circuit diagram of our model, but I found that if 55VCS and CS are connected together…
Part Number: LMV393 Other Parts Discussed in Thread: LM393LV , LM339LV Hello,
I just found out that the LMV393IDDUR is at end of time / last time buy. Now I try to find a direct replacement, but it seems that the package is really a problem.
It seems…
Part Number: LM393 Other Parts Discussed in Thread: LM339 , LM339B , LM339LV , TL331 , TL331B , TL331LV Hi team,
My customer is looking for 4ch comparator, they would need the spec is similar to LM393, could you please share some suggestion to us which…
Part Number: LM2901 Other Parts Discussed in Thread: LM339LV
Hi Experts:
Currently the project is planned to use LM2901DR as a comparator, if the supply voltage VCC provides a single +5V supply, IN+ is a fixed input of 0.5V reference voltage, and…
Part Number: TL391LV Other Parts Discussed in Thread: LM2903B , LM339LV , TL331LV , LM393LV , LM393 Hi Team,
We need a library file for TL391LV. I see a different model is available in the product page.
In folder i see LM2903B. Is it same for Tl391LV…
See the V CM /V ICR specification in the datasheet for what is guaranteed.
Do you really have signals between V CC − 2 V and V CC − 1.5 V? For 5 V systems, a low-voltage, rail-to-rail comparator like the LM339LV-Q1 would be a better idea.
I suspect that some input voltages exceed the valid common-mode range, which ends 2 V below VCC. What are the VCC and IN2+/− voltages?
If this is the problem, you have to use comparators with rail-to-rail inputs. For supplies not above 5 V, use the…
Other Parts Discussed in Thread: LM393LV , LM339LV I am looking for a comparator with low level absorption current up to 20mA output voltage up to 0.3V. Please recommend the following materials for packaging