Part Number: LM3409HV Tool/software: Hi,
We use the LM3409HV for the LED Drivers, and now, we have below issue:
1. The circuit spec: The input voltage of LM3409HV is 40VDC, LED voltage is 32V, LED current is 3A, the inductance is 10uH;
Our issue…
Part Number: LM3409HV Other Parts Discussed in Thread: LM3409 According to LM3409 datasheet, we used standard circuit , our application is input voltage is 12V, the output LED lighting is 6V, the current is 1A, the Roff=8K, the Coff=470pF, L=100uH, Rsns…
Part Number: LM3409HV Hi,
I'm building a led driver based on the LM3409HV trying to replicate an aquarium led driver (based on the same IC)
My driver works fine except for the intensity adjustment at low PWM levels.
The original driver has a "moonlight…
Part Number: LM3409HV Tool/software: I AM TRYING TO BUILD A 200WATT LED DRIVER USING LM3409HV
INPUT 61VDC OUTPUT REQUIRED 52.8 VOLTS 3.8 AMPS
PWM FREQUENCY 40KHZ
CAN SOME ONE GUIDE ME REGARDING THE DESIGN PARAMETERS WHAT SHOULD BE Fsw RIPPLE CURRENT…
Part Number: LM3409HV Hello,
Please check my design about LM3409HV?
The application is Heliport LED Driver.
LED module consist 5 series and 5 parallel. Each LED Vf is 3V and I want to driver it 350mA to 1A. (CREE/ XPGDWT-U1-0000-00E5E)
(But…
Part Number: LM3409HV Other Parts Discussed in Thread: LM3409 Tool/software: I am trying to design a LED DIMMING CIRCUIT using LM3409 HV
Vin 61 VDC
Vo 52 VDC
I LED 3.7 amps
this light is used for video / photography so there should be no visible…
Part Number: LM3409HV Other Parts Discussed in Thread: LM3409 Tool/software: This device has two operation modes: CCM and DCM. What are the conditions to transition from CCM to DCM?
Part Number: LM3409HV Tool/software: Hi TI Experts,
I am using the LM3409HV to design a 6A LED driver. Due to thermal concerns, I am considering using 2 or 3 MOSFETs in parallel.
My main question is: How many MOSFETs in parallel can the LM3409HV drive…
Part Number: LM3409HV Tool/software: Hi everyone,
I am using the LM3409HV driver to control LED current. The system generally works fine, but I am encountering an issue when I attempt to adjust the PWM signal (either increasing or decreasing the duty…
Part Number: LM3409HV Hi,
I'm designing an led driver to power a 0.75A 41.5V led board.
I've tryed to use the datasheet and the examples provided but I'm not sure about some components, expecially L1 and R sense.
On my protoboard I've used 18uH…