Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LM3410
Hi team,
Please help to review LM3410 schematic, the LED spec is also attached below. Thank you.
Every light bard is 5S9P. Customer ask us to provide the design tool to confirm the design parameters.
Regards,
Alex
Part Number: LM3410
Hi, Support Team
I am considering using LM3410. Would you please check whether LM3410 for 2 series circuit can support?
if 1pcs of LED vf:2.65v~3.1v for 2 series circuit; maximum current is?
if 1pcs of LED vf:2.65~3.1v for 4 series…
Part Number: LM3410 Hi,
I am considering using LM3410XQMF/NOPB LED driver in my project to drive a LCD backlight (which will be requiring 19.2V, 240mA).I am giving 5V as input voltage to the LED driver IC. I am planning to give 100% PWM to DIM pin for 24…
Part Number: LM3410 Other Parts Discussed in Thread: TPS92692 This is an 8-LED 5V input 350mA max output design.
Partlist exported from C:/Users/ERICST~1.BAN/AppData/Local/Temp/Neutron/ElectronFileOutput/83224/sch-5a5b68b7-665e-4f45-8b1f-9199d7c59e68…
Part Number: LM3410 Hello,
We are trying to replace the FAN5331SX in the schematic below with an LM3410 but the output goes to VIN and stays there. If possible, could someone please let us know if it is possible to create a 13v output with the LM3410…
Part Number: LM3410
This question has been asked before , but the answer did not offer a solution to the problem. I have a similar situation: LM3410 is driving white leds in parallel:
Vin: 5V
Vf (entire chain): 6.14V
Max current set at 0.5A
Dimming works…
Part Number: LM3410 Other Parts Discussed in Thread: TPS92613-Q1 Dear Sir/Madam,
I am considering using LM3410. Would you please check whether LM3410 is the proper part?
* Vin ; 5V * LED quantity ; 1 pcs * LED current setting ; 200mA * PWM brightness c…
Part Number: LM3410 Hi,
Do we have a spice model or something equivalent for the LM3410XMYE/NOPB? I checked TI.com and PSPICE for TI, but couldn't find anything.
Thanks!
Part Number: LM3410 Hi,
The customer is considering changing FAN5333BSX to LM3410XMF.
Please review whether LM3410XMF can be used for the existing schematic.
LCD backlight spec : IF=180mA / VF=9 ± 0.9V.
The FAN5333 can perform FB dimming.
Part Number: LM3410 Other Parts Discussed in Thread: LM3405 Hi Team, We want to design a valve driver (Shape memory) for one of our projects. The valve is a shape memory valve with a r esistance of 2.2 Ohms and a maximum rated power of 0.3W . The vale requires…