Other Parts Discussed in Thread: LM3431-Q1 , LP8860-Q1 , LM3410-Q1 , LM3410 , LM3423-Q1 , TPS92601-Q1 , LM3423 , TPS92691 Hello,
Are there any suitable device for the following specification? I think that LP8860-Q1, LM3431-Q1, LM3410-Q1 are similar with required…
Other Parts Discussed in Thread: LM3410-Q1 , LM3410 Hi, I'm trying to use the LM3410-q1 as SEPIC driver for an LED lighting. I noticed the DIMM pin is connected to Vin through a 100k resistor (in the example ), but that no DIMM label is used as is the…
Part Number: LM3410 Hi all,
I met some problems when using LM3410 in my design.
My design parameters:
Vin=5V;
Iin=300mA;
Iled=2.5A;
Vout=6.2V
and my schematic shows as below:
My question:
1 Should not R2 and R1 be connected to FB PIN? Is R1 1Ω or 1KΩ…