Part Number: LM3423 1. Pull down the lm3423 stick up pressure, it can't rise, abnormal (15V to 19v, pull down the lm3423 stick up pressure to 15V, it can rise to 19v if it doesn't stick up normally).
2. The LED is not on. The LED VIN and led…
Part Number: LM3423 Other Parts Discussed in Thread: TPS92690 , LM3424 , TPS92691 Can below LED driver IC use to design low side current sense?
⇒LM3423, LM3424, TPS92690
If any IC yes, please let me know about reference design, application note, etc…
Part Number: LM3423 Hello,
My customer is using LM3423 in BUCK mode and they found that the switching frequency will changing with the VIN pin voltage. Even the buck input is fixed, change the VIN pin voltage will change the switching frequency. Why is…
Part Number: LM3423-Q1 Other Parts Discussed in Thread: LM3423 , LM3421 Hi
Question on Buck-Boost Application ( Refer to datasheet "LM342x/-Q1 N-Channel Controllers for Constant-Current LED Drivers", SNVS574F –JULY 2008–REVISED JULY 2015)…
Part Number: LM3423 Other Parts Discussed in Thread: PMP15027 I am studying this LED driver for our driver monitoring camera and found below.
In the highlighted sentences, it states that RSNS can be neglected to be approximated the number of LEDs.
We…
Part Number: LM3423-Q1 Other Parts Discussed in Thread: LM3423 Dear TI,
We are going to build DRL with the LM3423-Q1.
We some question about LM3423-Q1.
1. What is the input / output tolerance rate? 2. ERROR AMPLIFIER: Under what conditions does the malfunction…
Part Number: LM3423-Q1 Dear TI,
For IC output characteristics Gain and phase margin should be measured in the operating area to satisfy the following requirements.
How do you measure?
Part Number: LM3423-Q1 Other Parts Discussed in Thread: LM3423 Dear TI Team,
Would you help this request?
I would like to know about the error range of Vout for the LM3423-Q1 product.
If the answer is difficult, is there a formula that can determine the…
Part Number: LM3423 Dear all,
I am using the LM3423 buck-boost evaluation board for testing a design. Ouput current goes unstable as Vin approaches the upper part of the range.
Vin: 7 V to 31 V Vout: 10.5 V Iout: 0.25 A PWM is to be used for dimming
At input…